Kevin Liao
- Total activity 11
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Activity overview
Latest activity by Kevin Liao-
Kevin Liao created a post,
[D457] Ma96712 + intel d457 in the Nvidia jetson platform
Hi I have an ODM project where the deserializer is a Max96712 connected to an Intel D457.I only see the source code for max9296 + max9295 in the master branch.May I ask if there is source code for ...
-
Kevin Liao commented,
I have fond root rause. I don't install udev package. Thanks your reply.
-
Kevin Liao commented,
Any updates?
-
Kevin Liao commented,
Yes, I have run them with sudo, and the result is still the same.The other machine, which installed version v2.55.1 a month ago, has both rs-capture and realsense-viewer working normally.
-
Kevin Liao commented,
I have successfully installed SDK version v2.55.1 using the following steps, but I’m still encountering some issues: When running rs-capture, the image appears, but an error is shown: xioctl(VIDI...
-
Kevin Liao commented,
Do I only need to make the following changes? If I only want v2.55.1 .Because the newer version of the SDK has many issues on our Nvidia Jetson platform."sudo apt-get install librealsense2-utils=2....
-
Kevin Liao commented,
I would like to know why, when I followed the same installation steps a month ago, the RealSense Viewer version was v2.55.1, but recently, using the same steps, the version became v2.56.5. Now both...
-
Kevin Liao commented,
I’ve tried running sudo ./rs-capture, but the issue still occurs. This issue only occurs in versions v2.56.5 and v2.56.4; it doesn't happen in earlier versions. I found that v2.56.5 and v2.56.4 wer...
-
Kevin Liao created a post,
Realsense SDK can'work on the Nvidia Jetson Jetpack5.1.4 (linux kernel 5.10)
Hi RealSense TeamPreviously, when I followed the steps below to install SDK, I was able to use rs-capture to stream video from the D457 GMSL camera.However, last week, after installing the SDK usin...