Disha Rathod
- Total activity 12
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 3
Posts
Recent activity by Disha Rathod-
Streaming Slowdown after a few hours on D415/D555
Set up: 2m shielded USB-C D415 camera The application streams depth, IR, color sensors and does minimal processing to detect anomalies in frames. Stream slows down after a few hours for seemingly ...
-
Realsense D555 Device not found error through ROS2
The D555 camera does not show up on ROS2 node. What is missing?1) Installed ROS2 Jazzy distrbution 2) Installed Realsense-ROS wrapper3) Built Realsense2 solution from source4) Wrapper version is 2....
-
Intel Realsense D415 Regulatory Certification
I have reviewed information available at https://realsenseai.com/regulatory-information/?q=/regulatory-information& This is not enough to satisfy our compliance department. How do i go about obtai...