Disha Rathod
- Total activity 12
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 3
Activity overview
Latest activity by Disha Rathod-
Disha Rathod commented,
Upgrading SDK had no effect on this issue. I would like to confirm if the 2.57 .NET wrapper has any known leaks?
-
Disha Rathod commented,
Application does have a memory leak climbing RAM usage in Task Manager; even after ensuring passing each intermittent frame to FrameReleaser and Disposing releaser at the end of every iteration did...
-
Disha Rathod created a post,
Streaming Slowdown after a few hours on D415/D555
Set up: 2m shielded USB-C D415 camera The application streams depth, IR, color sensors and does minimal processing to detect anomalies in frames. Stream slows down after a few hours for seemingly ...
-
Disha Rathod commented,
Yes, the Jumbo packet setting was the only missing setup. I was able to get the camera work after that. Thanks for your help!
-
Disha Rathod commented,
Also would like to add this is not resolved yet, I have reinstalled everything and built librealsense via colcon with -DBUILD_WITH_DDS=ON. Also enabled the LifeCycleNode. The node configure ends up...
-
Disha Rathod created a post,
Realsense D555 Device not found error through ROS2
The D555 camera does not show up on ROS2 node. What is missing?1) Installed ROS2 Jazzy distrbution 2) Installed Realsense-ROS wrapper3) Built Realsense2 solution from source4) Wrapper version is 2....
-
Disha Rathod commented,
MartyX Grover Yes, please provide further contacts for NDA procedure.
-
Disha Rathod commented,
MartyX Grover Is there any update on this?
-
Disha Rathod created a post,
Intel Realsense D415 Regulatory Certification
I have reviewed information available at https://realsenseai.com/regulatory-information/?q=/regulatory-information& This is not enough to satisfy our compliance department. How do i go about obtai...