Getomboy
- Total activity 16
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 1
- Subscriptions 6
Posts
Recent activity by Getomboy-
About make sure FOV specification of D435i
Hi, Nearly, we need to redesign the application of D435i. So we need to critical make sure FOV specification. Currently, using the resolution of 424*240 that approach FOV HD size. I've three quest...
-
About FoV issue of D435i
Hi, Recently, I use D435i to catch the point cloud data that have the unstable condition of FoV. The unstable condition is sometimes following FoV specification, but sometimes bigger than FoV spec...
-
About the camera connection issue on ROS
Hi Intel Support, I've a problem that about D435i load the log files to connect PC on ROS. I use the launch file to test the camera connection from the below address. (rs_camera.launch) git clone b...
-
How to synchronous control multi-camera without using series number?
Hi Realsense supporter, Currently I use the series number to control dual D435i cam. However, the device do mass production that cannot use the series number method. Because We cannot check every c...
-
How to filter the noise of D435i that the spotlight making ?
Dear Intel Service, When my camera turn the specific angle, the spotlight makes the camera noise (like flying pixel) to let my function failure. However, I cannot change the camera angle, it is our...
-
How to filter the (flying pixel) noise of D435i?
Hi, I'm using D435i camera on my AGV. Under the normal condition that FoV of camera is without occlusion, it has no noise on AGV working. (Shown as the below) When AGV with the shelf, FoV of camer...