Aznie Syaarriehaah
- Total activity 121
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 46
Comments
Recent activity by Aznie Syaarriehaah-
Hi Lucainnoc, The depth capture of L515 is starting from 0.25 to 9m and it performs best indoor with minimal exposure to the light. The maximum range of the L515 depends on laser power, receiver ga...
-
Hi S Coenders,The L515 LiDAR camera designed for indoor use. The performance will be degraded if the user points the camera towards the window during the day. In general, avoid brightly sunlit loca...
-
Hi Matthieu, Can you please share the screenshot of the Device Manager with the camera node expanded as shown in the attached picture? Make sure you connect to a USB 3 port. Regards, Aznie Intel...
-
Hi Kamal, That cannot be done. The coordinate system cannot be customized within the camera. Regards, Intel Customer Support
-
Hi Mdovrat,The Intel RealSense L515 Lidar camera connectors are USB-C 3.1 Gen 1 and the maximum length for USB 3.1 Gen 1 is only 2 meters. The cable provided along with the box is only 1 meter.If y...