Aznie Syaarriehaah
- Total activity 121
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 46
Comments
Recent activity by Aznie Syaarriehaah-
Hi Lyhour Newtechnology, The gaps in data between the aligned RGB and depth frames occur because the FOVs of the RGB and depth sensors do not completely overlap. By the way, in your previous reply,...
-
Hi Sandeep, You can refer to this article on how to sync the D435 via hardware. Hence, there is a whitepaper on External Synchronization of Intel® RealSense™ Depth cameras that might be helpful to ...
-
Hi Jesse,Can you try to update the firmware to the latest version? You can download the firmware from here. Also, please try to test the camera on another computer.Regards,AznieIntel RealSense Cust...
-
Hi Kenji Yasuda,I think there is an example for extracting the IMU data you can refer to for implementation details.Regards,AznieIntel Customer Support
-
Hi Lyhour Newtechnology,Have you tried to run the align-depth2color.py example? The bad depth image might due to the lighting condition of your space. Infrared light from the sun from windows can i...
-
Hi Sandeep,It is impossible to sync the RGB color frames for D435/D435i camera since the RBG and Depth Sensor are on different PCB. The D435 only has depth sync. There is no other version of the D4...
-
Hi Alessio Stella, There is only one model of L515 and you can check out the details on the Intel RealSense Store page. The tripod and the USB cable will come together with the box. Meanwhile, Real...
-
Hi Lyhour Newtechnology,The value represents the distance from the camera to the object. The L515 sends a laser beam and measures the returned time of the reflected light off an object. The L515 ac...
-
Hi Sjors, Sorry for the delay in replying to you. The maximum range of the L515 depends on laser power, receiver gain, object material, and ambient light. The camera can achieve its maximum possibl...
-
Hi Ming Ouyang, The bad depth measurement happened because of too much ambient light in the scene. The maximum range of the L515 depends on laser power, receiver gain, object material, and ambient ...