IACTICONTROL CTIcontrol
- Total activity 29
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 6
- Subscriptions 7
Posts
Recent activity by IACTICONTROL CTIcontrol-
Module and Processor board for D585
My question is really simple, will in a future be D585 modules and Processor boards as well as D455 or D435 have?
-
Depth module heat
Good morning: If I bought a realsense D450 module + Vision Processor Board D4 V3 to record/work for days. I am worried about the temperature of both D450 and D4 V3 board during intensive and long...
-
Use case for Depth module
Good morning: I'm about to buy some depth module in order to create an AI embedded system. I have 3 questions here: 1. Depth modules + boards are enough to work equals to camera asociated? For ...
-
Realsense intrinsic properties
Good morning: I want to put my Realsense D457 camera in some place, but maybe I will change his position. If i change his hight, orientation, rotation or any other movement, Will the following par...
-
Realsense D457 + Leopard Imagin + Jetson Orin Nano
Good morning: I have bought both LI-GMSL2-IPX-DESER and LI-FPC22-IPEX-ONX to connect Intel Realsense D457 via FAKRA GMSL to my Jetson Orin Nano. However, I need to build the drivers to connect the ...
-
Realsense D457 to Jetson Orin Nano with Jetpack 6.2
Good morning: I would like to connect mi D457 depth camera to Jetson Orin Nano without USB mode (therefore, I will use FAKRA/GMSL mode), How can I do it? I was searching some FAKRA board, but I am ...
-
Producto use of Realsense
Good Morning: I'm thinking on develop a product that use a Depth Realsense Camera/Realsense module with python. This product will use this Realsense camera and pyrealsense2 library to control all...