Charles Bursch
- Total activity 6
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 3
Posts
Recent activity by Charles Bursch-
Vision Processor D4 with MIPI connection to host
I am using the Vision Processor D4 ASIC on a custom motherboard design, and I'm using the x4 MIPI host interface (shown in figures 8-2 and 8-5 in the D400 Series datasheet) rather than the USB 3.1 ...
-
Weight of D455 Depth Camera?
What is the weight of the new D455 Depth Camera? The weight is not listed in the latest version of the datasheet.
-
USB2.0 required in addition to USB3.1?
I'm designing a custom computing PCB that two D415 or D435i cameras will be plugged into, and I will provide a USB 3.1 port dedicated to each RealSense. Are the USB 2.0 lines required to be present...