Shigeyoshi Ohara
- Total activity 18
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 6
Posts
Recent activity by Shigeyoshi Ohara-
D435 driver
Hello, I want to update D435 driver for Windows and found it in the page. However, it says it was deprecated and you should uninstall and download SDK 2.0. Is just installing Intel.RealSense.SDK-WI...
-
Infrared stream buttons don't appear in RealSense Viewer
Hello, When using with D435 on Windows 10 2019 LTEC, Infrared stream buttons don't appear in RealSense Viewer in 2 out of 4 systems. It seems to connect with USB 3.2. May I ask if someone would kno...
-
Do D435 driver and firmware support Windows 10 21H2?
Hello, A customer of mine asks if D435 driver and firmware already support Windows 10 21H2. If not, will you please tell me when they will support Win10 21H2. Regards, Ohara
-
intel-realsense-dfu detects D430 instead of D435
Hello, Connecting D435 to PC and run intel-realsense-dfu.exe, intel-realsense-dfu detects D430 is connected instead of D435. This happens with only some D435. Others are detected properly. Have any...