MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
If the callback error message is being generated from the librealsense file rs-processing.cpp as the link to Doronhi's comment earlier in this discussion states, then inserting some code for a reco...
-
You could use the RealSense SDK to convert a 2D color pixel to a depth pixel, find the depth value of the pixel and then deproject that pixel to 3D world points. https://github.com/IntelRealSense/l...
-
You could capture multiple people based on their skeletons using a single 400 Series camera with the RealSense-compatible commercial software packages Cubemos Skeleton Tracking SDK or the Nuitrack ...
-
Object detection systems based on trained objects tend to recognize objects based on their characteristics rather than their precise shape and dimensions. For example, in the RealSense 'Deep Neura...
-
I have not experienced Notch myself, though the Notch manual states under the heading Using multiple RealSense cameras with Notch that it supports up to four RealSense cameras. https://manual.notch...
-
Yes, the 400 Series cameras can work from behind glass. An example of this is a custom housing for the camera that an underwater project used. https://github.com/IntelRealSense/realsense-ros/issue...
-
Hi Antonio If you are using all cameras simultaneously on the same computer then four cameras is a good maximum to consider. For that number of cameras, a computer with an i7 processor or better ...
-
Hi Hamid Rezaie If you need to detect the pose of multiple boxes simultaneously instead of just one box then a DOPE approach based on ROS may be suited to your requirements. Such a system uses an...
-
Hi Yixun Liu The RealSense D435i and other 400 Series camera models such as D415, D435 and D455 continue to be produced. They can be purchased online from the official RealSense store for direct ...
-
The only demonstrated setting of frames_queue_size in the ROS wrapper is in the link below, where it is defined as a dynamic_reconfigure parameter. https://github.com/IntelRealSense/realsense-ros/i...