MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
It is possible to generate a master trigger pulse wirelessly with a signal generator instead of using physical sync cabling, though it can be significantly more difficult to achieve success than us...
-
If you are able to use C++ language and you only need static image capture rather than moving video then there is an existing multiple camera script created by a RealSense user that can capture an ...
-
Thanks very much for the visual confirmation. May I enquire please about the reason why multiple camera hardware sync is being used in your project. If the original intention was to sync FPS but h...
-
You can confirm please that pin 5 goes to pin 5 and pin 9 to pin 9, as shown below?
-
It looks as though you are using Ubuntu. Which method did you use to install the RealSense SDK, please? If you built the SDK from source code then you need to patch the kernel to enable support f...
-
Considering that the Inter Cam Sync Mode setting is in the Stereo Module depth controls, do you see any change if you have both depth and RGB enabled on both cameras?
-
The images are very helpful to see what is occurring, thank you. You are enabling RGB only and using modes 1 (Master) and 2 (Slave). However, Inter Cam Sync Mode 1 and 2 only support depth timest...
-
Hardware sync does not sync the FPS of multiple cameras, it syncs their frame timestamps.
-
As a general rule, if the casing of the camera is hot to the touch after only a few minutes after beginning streaming from a cold state then it could indicate a USB problem that is causing overheat...
-
In the clock images that you are capturing, are the timestamps of each camera visible in the image too?