MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
1. Yes, you do not need the UWP driver to use the RealSense Viewer. Detection of the camera is not dependent on the UWP driver, so there may be some other issue that is preventing detection. If y...
-
Does it flip if you set Y rotation to '180' instead of '0'?
-
Hi Vera Halavach Whilst some products in the RealSense range are discontinuing, the 400 Series stereo depth camera range is continuing. The models being discontinued are L515 (lidar depth camera)...
-
Hello, a rough workaround for flipping an image in Unity can be to find the Unity material responsible for displaying a texture and give it a minus value for its scale in the material's scaling set...
-
Another RealSense user recently experienced problems (though not with UWP) when their Windows build was updated from 1909 to 2004 https://github.com/IntelRealSense/librealsense/issues/9698#issuecom...
-
As it is an .inf driver that is being installed, I wonder if you need to be logged into Windows with a user account that has Administrator privileges for security reasons. Is the Windows computer ...
-
Hi Eriko Mogi The RealSense UWP driver only needs to be installed if you widh to interface with hardware or software that supports Microsoft's Universal Windows Platform (UWP), such as the Microso...
-
There is very limited information available on the subject of the hardware sync pins outside of the multiple camera guides and no waveform images that can be found, so there is not much that I can ...
-
Hi Bessmagsm If your problem is that your camera cannot see in low light in RGB mode, if you have a D415 or D455 camera model then you could try capturing color from the left infrared sensor inste...
-
Hi Mhm Nab 400 Series stereo depth cameras are widely used in commercial and industrial applications. The Use Cases page of the official RealSense website provides examples of applications in dif...