MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
The structure of the ethernet networking open-source white paper can admittedly be difficult to follow. Instead of using the librealsense installation method on the libuvc_installation.md page, I ...
-
Are you able to connect to the camera with Add Network Device if you SSH into the Ubuntu computer and input the command sudo systemctl restart rs-server.service to restart rs-server as described in...
-
Hi Gbi The RealSense 400 Series cameras can make use of ambient light in a scene to analyze surfaces for depth detail. In a dimly lit scene though, enabling the camera's IR Emitter component to p...
-
Translation: Thank you very much. I succeeded in changing the firmware. However, I still couldn't set D415 and file transfer on my Android smartphone. On my HUAWEI P30 lite, I have enabled USB ...
-
Hi Aron If the Projector temperature of the camera is detected to be less than 0 degrees C then the laser safety mechanism in the camera firmware driver shuts off the laser. This does not prevent...
-
Hi Shigeyoshi Ohara Most of the packages are not large in size and so there is no harm in just clicking Next to install all suggested options. If you do need to reduce the install size then when t...
-
Hi Laszlo Csabi Could you check whether installing the IntelliSense language extension module for Python in the link below resolves your problem with code completion not appearing for pyrealsense2...
-
Hi Laszlo Csabi There is not a method in the Python wrapper for splitting bag recordings by duration (ROS can do it with the 'split' function of its rosbag record bag recorder). You could though ...
-
Thanks very much Rohit for the update - it's great news that you were successful. :) Good luck with your project!
-
I believe there is some flexibility with the value when the tool is checking whether the requested orientation has been met. The Y value of '-0' when -1 is requested seems unusual though. Have yo...