MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Rohit Page 61 of the current edition of the data sheet document for the 400 Series cameras lists the product codes of the D455 models that contain the two types of IMU component. https://dev.in...
-
3 meters is a relatively short extension length. So whilst it is important to use a high quality cable for lengths greater than 2 meters, you are less likely to have problems than a cable that is ...
-
Hi Viseshsonigra What is the length of the USB cabling that you are using, please? When using your own choice of USB cable, the cable can have poorer performance compared to the official 1 meter...
-
Hi Pedro Gomezgarcia In the Dispostivos de imagen section of the Device Manager, please right-click on the SR300 Depth driver and select the Uninstall option. Unplug the SR300 camera and wait a c...
-
Hi Sagar It is unusual that you received the error OPENSSL_ROOT_DIR (missing: OPENSSL_CRYPTO_LIBRARY OPENSSL_INCLUDE_DIR) on an Nvidia Jetson, as it usually only occurs on Apple Mac installations....
-
And the same timeout is produced in the Viewer if you install an earlier version of the full RealSense SDK such as 2.48.0 using the Intel.RealSense.SDK-WIN10 automated installer file? https://git...
-
Are you able to connect the Windows version of the Viewer to the Ubuntu remote computer if you download and run the standalone version of the Viewer called Intel.RealSense.Viewer.exe from the 'Asse...
-
Thanks very much BaLinZhu for your patience. The Windows version of the Viewer should certainly be able to communicate with Ubuntu. The IP address entry box for the Add Network Device option expl...
-
IGNORE SPAM ADS ABOVE
-
After connecting to the device through a remote terminal with ssh (Linux) or Putty (Windows), you confirmed at the start of this case that you have set the static IP as described in the section of ...