MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Kamyar The links below highlight two past cases of the issue that you encountered with the 848x480 resolution being unsupported but the other resolutions being unaffected. In the first link, t...
-
If you are only using RGB then distance from the object should not be so much of an issue. To demonstrate this I used a D435i to capture keyboard keys at 1, 2 and 3 cm height from the keyboard res...
-
It is also worth highlighting that there are solutions for scanning with a single camera by moving the camera around a scene and progressively building up the detail of the scene on the scan. A fr...
-
Hi Wuhairongqq 1. In general you may wish to position the three cameras so that their field of view (FOV) overlaps with one another. This will help to avoid blind-spots in the observation of the ...
-
Hi Chandannaik999 I do not have an exact figure for hyperfocal distance (the distance below which the image can become blurred) when performing close range sensing. On the D435 / D435i models tho...
-
The changes in firmware versions are typically minor. So it is practical to select a firmware and then not update for a period of months (such as every six months) without missing anything vital. ...
-
If you need to use a single PC and you will be using camera settings that will result in high data volumes, and you will be connecting the cameras to a USB hub, that could result in there being ins...
-
I would recommend SSD because of its improved access speed compared to older HDD technologies such as SATA. If you will be recording camera data in the bag file format then a large drive is recomm...
-
If the camera is being used in a high temperature environment then warming of the camera's outer casing may cause an internal temperature rise. As an example of this relationship between outer and...
-
Hello, it is fine to use a 5 meter USB cable with RealSense cameras if the cable is a high quality one, otherwise you may experience degraded performance or disconnections. The company Newnex supp...