MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Cedric Vanloon The 1920x1080 image looks blurred compared to the 640x480 one. Did you manually resize the 640x480 image or did you use the Snapshot button in the top corner of the Viewer windo...
-
You mentioned that the RealSense Viewer program worked fine, suggesting that the camera and the RealSense SDK installation in general is okay and that the problem is with the pyrealsense2 installat...
-
Hi Begaiym Kudainazarova Which RealSense camera model are you using, please?
-
There are RealSense applications where you can simply substitute in an updated version of the RealSense DLL. For the RealSense Viewer though, to use an updated version you should either update the...
-
Hi Ddfleck Yes, when I saw that you were using MacOS 12.0.1 I thought that the non-detection of the camera may be related to the USB issues with Monterey discussed on the RealSense GitHub support ...
-
It was a good idea to update your firmware from 5.9.13 to the recent version 5.12.13.50 first before using 2.50.0. Can I confirm whether you are updating the entire RealSense SDK by downloading...
-
2.39.0 dates back to October 2020. The SDK is now at 2.50.0 at the time of writing this and there have been a huge number of updates and bug fixes made to the SDK since 2.39. So if you are able t...
-
I would think that the link that you used to build the wrapper may have installed the latest version of the wrapper - 2.3.2 - for SDK version 2.50.0. https://github.com/IntelRealSense/realsense-ros...
-
Hi Eriko Mogi There have been a couple of past cases of this error, such as the one in the link below. https://github.com/IntelRealSense/librealsense/issues/1930 If you are using Windows, please c...
-
Hi Varsha 11891 The first thing to bear in mind is that the D415 camera model does not have an IMU motion tracking component like the RealSense D435i and D455 models do. So whilst the rtabmap_ros...