MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Thanks very much Begaiym Kudainazarova for the update. Are you still having the same problem with Jupyter Notebook, please?
-
The FOV for the D455 in the data sheet matches with the depth FOV for that model in the RealSense Store specification listing and with Intel's camera model comparison chart at the link below. https...
-
Hi Ilya Nax Could you try running the Windows rs-capture.exe example program using the instructions in the link below please to see whether the RGB stream is provided in that application? https:/...
-
RealSense 400 Series cameras can work with any Intel or Arm processor. The same assurance is not applied to AMD processors though. Whilst there have been a few past cases where Ryzen / Threadripp...
-
Can you confirm which computer / computing device you are using with the camera, please? In my previous comment, I suggested that if you are using a single-board computing device such as Raspberry...
-
If all 12 cameras on one computer were going to be active at the same time then you would need a powerful computer because of the amount of computing resources that 12 cameras would consume (it is ...
-
How about a column with a very heavy base that could have a camera attached to it via a tripod thread, such as the Elgato Multi Mount equipment in the link below (the 4.8 kg heavy base is in the Ac...
-
Examples of 3D printing blueprints for mounts for D435 can be found at websites such as Thingiverse, Yeggi and GrabCAD. https://www.thingiverse.com/search?q=realsense&type=things&sort=relevant http...
-
The CONIX Research Center at Carnegie Mellon developed a C++-based system for generating point clouds from up to 20 RealSense cameras and then stitching them together. https://github.com/conix-cent...
-
Multiple 400 Series cameras do not interfere with each other. MeshLab and Pyntcloud (for Python) are examples of free / open source software that can convert a .ply point cloud file into a solid ...