MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
When building from source, the most recent configuration supported in SDK version 2.50.0 at the time of writing this is Ubuntu 20.04 and kernel 5.11. The SDK is able to work with newer kernels but...
-
I do not need logs at this point, thanks. The most recent Ubuntu version that the RealSense SDK is officially compatible with is 20.04. Did you test the camera with 20.04 or 20.10 in September 202...
-
Hi Orflyfisher82 Which OS are you using the camera with, please?
-
You are very welcome!
-
Hi Andi Forster My first thought for an approach to this problem would be to alter the frame queue size to add latency and reduce the risk that frames are dropped. Changing the frame queue size a...
-
It may be worth testing the RealSense SDK's rs-grabcuts OpenCV C++ example, which also aligns depth and color, to see whether the same problems occur when running that program on your PC and Jetson...
-
As mentioned earlier in this discussion, even if the camera hardware is fine the camera may work on some PCs but not others. Reasons for this could include a problem on the USB ports of the comput...
-
Thank you very much for confirming your camera model as a D435i stereo depth camera. Intel have a RealSense camera tuning guide at the link below that is a very good reference for advice on achievi...
-
Sometimes doing a complete wipe and reinstall (including reinstalling the OS) can suddenly resolve a problem if everything else that has been tried to resolve that problem has failed.
-
Hi Dev Luenah May I first confirm which RealSense camera model you are using, please. The question is tagged as D400 Series but lidar is mentioned. The 400 Series cameras are Stereo Depth techno...