MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
In the second link, the RealSense user in that case shared their Qt project. https://github.com/ZiSo89/QtIntelRealSense
-
Hi A Salhi I recommend studying the links below as a starting point for creating a RealSense application with Qt 5. https://github.com/IntelRealSense/librealsense/issues/6649 https://github.com/Int...
-
There is detailed guidance on page 8 (the final page) of the PDF document linked to below regarding using the RGB of the D455 model specifically in bright sunlight. https://www.intelrealsense.com/d...
-
Hi Hamid Jebliouazzani 1. Yes you can use D455 with USB 2.0. The range of supported resolution and FPS modes will be more limited than on a USB 3 connection though. For example, at 1280x720 reso...
-
Hi Steve Steve No plans have been announced to discontinue the RealSense 400 Series stereo camera range and new models D401 and D405 were recently released. The End of Life notice was in relation...
-
The Y16 infrared stream is unrectified because it is used for camera calibration. It has a smaller number of supported resolution and FPS modes than Y8 though.
-
Hi Henry, the D401 / D405 have hardware differences to the other 400 Series stereo depth camera models that make them capable of sub-millimeter accurate, high quality images at very close range. ...
-
Hi Nati Farkash Intel have a RealSense OpenCV tutorial for doing this at the link below. https://github.com/IntelRealSense/librealsense/blob/master/doc/stepbystep/getting_started_with_openCV.md
-
Hi Lucan Martin If your application does not have to depth-sense further ahead than 0.5 meters and does not require an IMU or the IR Emitter component then the compact-sized new RealSense D405 may ...
-
Hi Dzhus Thanks very much for your questions. 1. Depth measurement error starts at around zero at the camera and increases linearly over distance. This phenomenon is called RMS Error. On the D43...