MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
I thought that there was a possibility that this might occur, since the overlaid coordinate writing is applied to the color image within a loop at the part of the box_dimensioner_multicam script li...
-
Hi Javi0798 I would speculate that you could create a function that is called when a button-click event occurs, and save the color image with the OpenCV imwrite instruction. Assuming that you wil...
-
It should work automatically with USB 2.0 without having to make further adjustments. I was able to replicate this problem with a D435i on USB 2.0. It was apparently a problem that was specific to...
-
A RealSense calibration specialist from Intel has read this case and will be posting expert advice for you on this discussion.
-
Hi again Mcui The back in stock status of the HSF Flexi Interposer cables in the RealSense Store has now been updated to the end of May 2022.
-
Hi Ron Vis Yes, RealSense 400 Series cameras such as the D435i model can be used with USB 2.0. When the camera is inserted into the USB 2.0 port, does Windows make the "doo doo doo doo" USB devi...
-
It looks as though the dot pattern is sufficiently visible to provide a texture source for the camera to analyze for depth information. At 500 mm range, you may get more accurate results if you set...
-
Please provide an infrared image of the wall so that I can see how visible the dot pattern projection is on the wall surface at 500 mm range.
-
Technically the optimal depth accuracy resolution is 848x480 on the D435i, though depth precision increases as resolution increases. So is there any positive change if you increase resolution to 1...
-
How does it perform if you set Second Peak Threshold to '0' instead of the default '325'