MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
There is a certification document for the SR300 that can be downloaded from the link below. I hope that it will be helpful to you. https://drive.google.com/file/d/1IifonkLEmLYtUeTxo-5PjdaL0Z-Fq7sV...
-
If you build from source code with the RSUSB backend method then you can build for a range of different flavors of Linux. An RSUSB build of librealsense bypasses the Linux kernel and so is not dep...
-
Hi Roberto Mangano Would it be possible to update your product to use a RealSense 400 Series camera or depth module board, as these have IEC60825-1 laser safety certificates available for download...
-
I am not aware of a direct download link. My understanding is that if the librealsense SDK is built from source code instead of installed from packages then the librealsense2.so file will be locat...
-
In terms of librealsense, .so will typically refer to a package installation of the librealsense SDK rather than a source code compilation of it. https://github.com/IntelRealSense/librealsense/blo...
-
Hi Tiago May Do you have auto-exposure enabled, please? If you do then it is good practice to skip the first several frames after the pipeline is started to give the auto-exposure time to settle d...
-
There was a recent case at the link below where an LED was being measured at 60 cm distance from the camera and they were experiencing "depth jitter" variation in the measurements. Their depth ima...
-
Hi Chantrapornchai The RealSense LabVIEW wrapper is designed for Windows 10. I am not aware of any cases where it has been run on Linux, though a RealSense team member who was once asked if it co...
-
Hi Renaud Bastien The camera can have difficulty reading depth detail from reflective surfaces such as the glass of fish aquariums. If the camera is outside of the bowl then aligning depth to col...
-
Raw frames are the original ones generated at the point of capture (the camera) before they undergo processing such as having a distortion model applied by the camera hardware and are then sent alo...