MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
You are very welcome! You are correct about Mode 2, it will still stream in the configured FPS whether sync is active or not. In regard to your further questions: 2. RGB is not synced in gen...
-
Mode 2 listens on every frame, so it would be the same period of time no matter which FPS rate is set. AS far as I am aware, the precise wait period on each frame has not been defined. The origi...
-
The camera will generate depth data for whatever areas of the scene that the cameras can see in the FOV and analyze for depth. If part of the FOV is obscured then this does not prevent the generat...
-
Hi Yixun Liu The stereo baseline is the distance between the center-lines of the left and right sensors. As these physical sensor positions are fixed, the baseline cannot be changed.
-
Hi Roman Leuzinger The field of view (FOV) of the camera module's sensors should not be obscured by any non-transparent part of the custom housing that is on the front of the housing. If you are...
-
HI Yixun Liu If you wish to illuminate the scene with infrared light but do not need the dot pattern, the best solution for you may be to change the value of the Laser Power setting. This affects...
-
The RealSense Viewer has a range of post-processing filters enabled by default. So you could test your theory by left-clicking on the blue icon beside Post-processing in the Viewer's options side-p...
-
Hi, I recommend the advice at the link below if you have not seen it already. https://github.com/IntelRealSense/realsense-ros/issues/2084#issuecomment-1324768610
-
If you are using the RealSense Viewer tool then depth and color are not aligned in its '2D' mode. Also, aligned data cannot be saved to a bag file. Instead, individual streams (such as depth an...
-
Hi Patnisrj22 This is a limitation of the RealSense Viewer tool's Threshhold Filter interface, not the D455 specifically. The maximum settable distance of the filter is 16 meters no matter which ...