MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
The USB standard permits as many as five USB hubs to be linked together in a 'daisy chain'. My research of the subject indicates though that devices spread across more than one hub may receive ins...
-
Hi Jingliang Tian Which version of the RealSense SDK or RealSense Viewer are you using, please? Firmware 5.17.0.10 is designed for use with SDK / Viewer version 2.56.5 or newer.
-
Steve Steve 50 degrees does seem excessive in a cool room. Electronics may heat up more if they are used in a geographical location that is high above sea level, because the air will be thinner ...
-
The official estimate of accuracy for the D435i model is <2% at 2 m so that should be your expectation, and RealSense cameras are usually already well-calibrated by default when received by the cus...
-
I have seen cases where a company has a team perform their own custom calibration of newly received stock of cameras before integrating it into their product. So using On-Chip and Tare certainly i...
-
A non-RealSense Intel document at the link below about the Above Threshold field in an MDDS document states that "Under the RoHS table, the False response to the Above Threshold (T/F) query indicat...
-
Hi Ryosuke Tajima The link below has guidance from RealSense D555 users and from one of my RealSense colleagues with D555 expertise that may be helpful with your issue. https://github.com/IntelRea...
-
You are very welcome! I do not have a time estimate regarding when the next D555 datasheet update will be but have made a note to post a message on this thread when it is released.
-
Hello, an Invalid SKU error indicates a problem with the firmware driver. On a D455 this could be caused by installing a firmware version older than 5.13.0.50, as that is the minimum firmware that...
-
RealSense cameras have been tested for long-run use and can be active indefinitely so long as their internal temperature remains below recommended limits. The 36.9 degrees that you reported the ca...