MartyX Grover

  • Total activity 2417
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 1 user
  • Votes 1
  • Subscriptions 745

Comments

Recent activity by MartyX Grover Recent activity Votes
  • Thanks very much for the detailed test feedback from use of the engineering firmware.  I will pass it back to my RealSense colleagues who provided the firmware to seek further advice.  Thanks for y...

  • Which firmware driver version is installed in your camera, please?  If it is a new camera that has not yet had its firmware updated then its firmware may be out of date and not recommended for use ...

  • My colleagues tested on Jetson Thor and were not able to reproduce the reported IMU oscillation.   In their test, they launched the ROS2 wrapper with ros2 launch realsese2_camera rs_launch.py and e...

  • If all streams on the camera are otherwise working normally and the error message is not generating continuously then I would recommend ignoring the message.  For some error situations, they are on...

  • Please provide information about the questions below.   1.  Which version of the RealSense SDK are you using the camera with?   2.  Has RGB ever worked since the camera was purchased or did it work...

  • Hi sara ponzetti  If you are able to enable the depth stream in the RealSense Viewer tool, please first try resetting the camera to its factory-new calibration values using instructions at the link...

  • I can only advise about RealSense cameras, and D405 is the only close range RealSense camera that can work at this very close distance from the object.

  • Thanks very much for the new data.   A Y-axis Accel value of 9.7 to 9.8 usually indicates that the IMU is well calibrated and does not need recalibrating, as the ideal target value for Y Accel is 9...

  • Hi eva mu  I performed depth measurement tests with a D405 with a white object with a similar shallow indentation.  With certain settings it was possible to have the cavity visually display as a di...

  • The NCS2 (Neural Compute Stick 2) USB acceleration stick was able to be used with RealSense 400 Series cameras years ago to provide hardware acceleration for applications.  It contained an Intel Mo...