MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Richard Do you require further assistance with this case, please? Thanks!
-
Does detection during ROS wrapper launch become any more reliable if you add initial_reset:=true to the launch command to reset the camera at launch? Is it detectable if you launch the wrapper no...
-
To use librealsense applications such as realsense-viewer on a DDS connection, it should be necessary to build librealsense from source code with the -DBUILD_WITH_DDS=ON flag. In regard to ROS2...
-
Hi JIshnu S Alignment is a processing-intensive operation and so it is recommended that Nvidia Jetson users enable the librealsense SDK's CUDA support to offload alignment processing from the Jets...
-
The recommended method of installing the librealsense SDK for use with DDS is to build it with source code with CMake using the 'installation.md' instructions and include the flag -DBUILD_WITH_DDS=...
-
Hi Niklas Schlueter Launching the ROS2 wrapper in D555's DDS ethernet mode is supported. If your camera has firmware driver. I note though that you are using librealsense and wrapper versions th...
-
Using manual exposure values can be tricky, as setting the exposure in a certain range could cause a drag on the FPS speed so that FPS is lower than the setting that you defined. For manual expo...
-
Hi JIshnu S At that motion speed it would likely be a rolling shutter issue. Lag between depth and RGB caused by the D435 RGB sensor's slower rolling shutter can be compensated for by using 2x th...
-
Hi LUCAS DI FRANCO I have responded to your question at the GitHub version of it. Please continue the support discussion there. Thanks! https://github.com/realsenseai/librealsense/issues/14994
-
If you are generating a pointcloud with your application then I recommend checking that the pointcloud object is not being created within a loop, as this can cause a memory leak. Advice about this...