MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
When calibrating the IMU with the Python calibration tool, the outcome of the calibration can be negatively affected if the camera is overly tilted when orientated in the vertical position (USB cab...
-
I knew that a RealSense user had previously produced a raw disparity map by accessing the camera hardware directly, and managed to track down the script solution that they posted for doing so. http...
-
My advice would be that if disabling RGB is found to consistently resolve the issue on your particular computer then do that, unless RGB is vital to your project. Having the infrared stream active...
-
How does the depth and IR behave if RGB is disabled?
-
Judging by the IR image, it looks as though the band is produced by a second partial image-slice being generated at the top of the screen, with a gap between the main image and the partial one. I ...
-
Hi Yzkzero If the Right MIPI error has only occurred several times in a 2 month period and you can clear the problem after a hardware reset, and you can stream normally the rest of the time, then ...
-
The rs-motion documentation explains that gyro drift may occur if the alpha value is too high. Using a lower alpha value shifts the balance of the calculations to favor the accelerometer instead o...
-
Thanks very much. I will not be handling that case. One of the Intel Support team members on this forum should pick it up. Good luck!
-
The best way to proceed may be to create a new post on this forum, asking for a Feature Request about setting up the valgrind feature that you have described above. It is not something that I mys...
-
I do not have any further librealsense information about valgrind. You can define a custom suppression list in valgrind though, according to its documentation. https://www.valgrind.org/docs/manual...