MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Thank you for the confirmation. Next, let's eliminate the possibility that the Windows privacy settings have somehow enabled and are preventing access to the camera. Please follow the instruction...
-
Hi Jinshiksung As a starting point in investigating your problem, can you confirm please that your D455 is still not detected after you have completely shut the computer down and then restarted it...
-
Hi Getomboy You do not need to know the serial number value of each camera, as the query_devices command can check all of the cameras that are currently connected and use the information stored in...
-
Hi Saad Azhar The amount of motion in the water will likely be within the capabilities of the camera to register if the water is churning round. Even in 2015 with an original-generation RealSense...
-
Yes, a signal generator can be used, with an example of such a setup shown in the image below (which features an Arduino Micro with a level-shifter to bring the sync signal to 1.8V). A member of t...
-
You are very welcome Shimamoto1991 - I am pleased that I could be of help!
-
Which method did you use to install the RealSense SDK on Windows, please? Did you go to the SDK Releases page and use the automated installer file? https://github.com/IntelRealSense/librealsense/b...
-
software_device is going to be your main option for feeding OpenCV data to the librealsense SDK. It should not matter if you do not have access to rs2 depth frames, as the purpose of software_devi...
-
Thanks very much for your patience. Next, please unplug the micro-size end of the USB cable from the side of the camera, turn it upside down and re-insert it (USB-C cables are two-way insertion on ...
-
If your aim is to convert a cv::mat to rs2::frame, does the cv::mat conversion process referenced earlier in this discussion not provide this ability in a way that fits your project, please? https:...