MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Lalatendu Das Another RealSense user who was attempting to use software_device in Python encountered the same problem with create_matcher in the case linked to below. They were not using synce...
-
I would expect there to be differences between models regarding the extrinsics between sensors. This is demonstrated by the three images below, from a D435i (top), D455 (middle) and D415 (bottom)....
-
1. Given that your updated chessboard was measured as having a square size of 2.6, did you set the square size in the script at the meters-value of 0.026 https://github.com/IntelRealSense/libreals...
-
I can understand why the rotation and translation extrinsic values would be hardcoded values in rs-software-device since the software-device system is used to simulate camera hardware, and so there...
-
Hi Leila, welcome back! The dots on the infrared view are generated by the IR emitter of the projector on the D435i camera. The projector casts a pattern of semi-random dots onto the scene observe...
-
Hi Yixun Liu Are you using the camera on a USB 2 connection please? If you are then Infrared 2 is unavailable in that mode and only Infrared 1 is supported. Infrared 2 requires the camera to be...
-
Great news about your success with the conversion! Conversion of numpy to rs2::frame is something that other RealSense users have explored. As far as I know though, a definitive solution for doing...
-
Hi N Kanbe I9 If you are using the RealSense Viewer tool and your depth range is limited to 4 meters then it may be because a post-processing filter setting called the Threshold Filter is enabled....
-
I believe that in C# the device connection status can be checked with OnDevicesChanged https://github.com/IntelRealSense/librealsense/issues/3142#issuecomment-465494716
-
A C++ user reported a similar memory leak pattern with Visual Studio 2019 in January 2020. In their report, D435 displayed the same flat constant pattern as your D435, but D435i and D455 had the u...