MartyX Grover

  • Total activity 2417
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 1 user
  • Votes 1
  • Subscriptions 745

Comments

Recent activity by MartyX Grover Recent activity Votes
  • Please right-click on the Intel AVStream Camera 2500 driver and select the Disable device option to disable this camera (you can re-enable it again at any time if you need to by right-clicking on t...

  • Thank you.  Could you open the Windows Device Manager interface and check under its Cameras category for whether there are two RealSense drivers there, a Depth driver and an RGB driver.  

  • Thank you very much.  The white display does not look like a typical Frames Not Received scenario, as those words would be displayed in red lettering at the center of the RGB panel if it were.  It ...

  • Hi Simeonb  Could you left-click on the small up-arrow in the bottom corner of the Viewer window please to open the Debug Log interface and then activate the RGB stream and let me know what the log...

  • The depth and RGB exposures use different scales of value, with large values for depth exposure (default 8500) and small values for RGB (default 156). I located a reference in the librealsense SDK'...

  • Next, could you try disabling the GLSL options in the Viewer's settings using the instructions in the link below to see whether it makes a positive difference to performance. https://github.com/Int...

  • If you are searching for developers who can provide solution development services, the website at the link below may also be helpful. https://www.intelrealsense.com/development-service-vendors/

  • Hi Cristian Vilar  My understanding is that the unit of exposure is in milliseconds (ms) and its value can be controlled with microsecond (usec) granularity.   https://github.com/IntelRealSense/lib...

  • I ran depth + RGB tests in version 2.45.0 of the SDK (the one that you are using) and found it far more difficult to generate a frame drop by doing so than in previous SDK versions, whether Auto-Ex...

  • I note that in the image of the RGB section above, you have RGB Auto-Exposure disabled (black box beside it).  Auto-Exposure is not the same as Auto-Exposure Priority (which does need to be set to ...