Gbenel

  • Total activity 19
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 4

Posts

Recent activity by Gbenel Recent activity Votes
  • Is Depth/Color alignment needed for the D455 like it was for D435?

    Just got a new D455 to use in place of a D435. Is it necessary to align depth and color streams using align.to as it was for the D435? Reading through the promotional material for the D455 I am und...

  • D455 + T265 3d print mount?

    Hi All, Just got the new D455 realsense camera. I have been using the D435 in conjunction with the t265 using the 3d printed mount for both cameras from the CAD file that was provided a while ago. ...