Lab
- Total activity 19
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 5
Posts
Recent activity by Lab-
Realsense D435 on network with rasperry pi4
Hi, I'm trying to use this setup:https://dev.intelrealsense.com/docs/open-source-ethernet-networking-for-intel-realsense-depth-camerasIt seams to work. I had to install realsense viewer V2.48 (in t...
-
D435 - Camera Protection or Custom Firmware
Hi! I need to lock the camera to my software (in python). I want that in my NUC (with linux), only my software can use the D435 connected... Is it possible to do that? If I can customize the firmw...
-
D435 external temperature
Hi everyone!I'm usinga lot of Intel realsense d435 for a project and after a few minutes they become a lot hot! I can't even touch them!Is this normal? are there any way to avoid that?Is it safe to...
-
D435 and D415 skeleton tracking, similar to Kinect
Hi everyone! I'm trying to replace the kinect v2 in some projects of mine.I'm testing these two cameras (D415 and D435) with Nuitrack. It's ok, but I want to try something else...Are there other sk...
-
D435 case and front cover material
Hi everyone! I need to install my d435 camera in the wall (inside a hole) and i would like to close the "hole" with a glass or a transparent plastic. What material can I use to cover the front of...