Jerry
- Total activity 25
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 6
Posts
Recent activity by Jerry-
How to get actual Infra Red image with 415
Hi ! Has anyone managed to get an actual IR image without any of the visible light ? The example in the SDK (Unity wrapper) is a mix of both I think as I can read the print on books that I hold in ...
-
415 depth sense granularity
I'm projecting onto a surface and using the 415s point cloud to sense objects on it (because point cloud allows depth cutoff and the 2d doesn't - in the unity wrapper anyway) Here's my setup - 3 vi...
-
Sense hands on table when realsense 415 & projector are fixed above.
Hi - I've got the 415 realsense sdk 2.0 working within Unity which is great and v. colourful. I'm building an interactive table like the picture below, and am hoping to use the realsense to work ...
-
Cursor Mode on D415 with unity build
Hi, Can anyone tell me whether I will be able to use the Cursor Mode with this model as mentioned at 1:48 in your video here - (https://www.youtube.com/watch?v=pjEtpwEfTaw) as I can't find document...