Cursor Mode on D415 with unity build
Hi,
Can anyone tell me whether I will be able to use the Cursor Mode with this model as mentioned at 1:48 in your video here - (https://www.youtube.com/
Also if it IS still usable, what is the maximum touch points it should be able to detect ?
any help would be Vastly Appreciated.
-Jerry
-
Cursor mode was part of an older SDK from 2016 that is unfortunately not compatible with the D415 camera.
If you want to use hand tracking with the D415, the best tracking solution currently available is commercial software called Nuitrack SDK. Its license price is $39.99 a year, though it has a free trial version too.
Please sign in to leave a comment.
Comments
1 comment