MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
I cannot find the original case link but there was not much information on it. The camera whose hardware was affected by a period of storage was simply shipped by post from India to Intel by the u...
-
Aside from a high temperature event or vibration, a camera can also become mis-calibrated if it receives a physical shock such as a hard knock or a drop on the ground. It does not sound as though ...
-
Hi Toni Divic There was a past case where a RealSense camera stopped working correctly after being in storage for a couple of weeks and then recovered itself whilst being shipped by post to anothe...
-
Hi Deepaksharma848586 The link below has guidance about installing librealsense and the pyrealsense2 wrapper on Raspberry Pi. https://github.com/IntelRealSense/librealsense/issues/11506#issuecomme...
-
Some other volume estimation methods can be found here: https://support.intelrealsense.com/hc/en-us/community/posts/5606479919379/comments/5609636432915
-
Hi Ttbinh12122002 The RealSense SDK has a Python example program called box_dimensioner_multicam.py for calculating the volume of an object (length, width, height). https://github.com/IntelRealSen...
-
Hi Harry Ty Hu The depth image is not constructed from the infrared streams that are accessible to RealSense users, but is instead constructed from raw infrared frames inside the camera hardware a...
-
It should be okay as the D405 would not be able to see IR light frequencies.
-
Hi Cuau Lenaic The RealSense D405 camera model cannot see the near-infrared light spectrum because the sensors are equipped with an IR Cut filter and so it can only see the visible light spectrum....
-
This site would not allow the links to be posted so I have provided them as an image so that they can be manually typed into your web browser address bar. My apologies for the inconvenience.