MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
https://github.com/IntelRealSense/librealsense/issues/5038#issuecomment-541289841
-
You are very welcome. It's no trouble at all. :) If you need to use a longer USB cable then the cable should be a high quality one designed for handing data transfer. If the length is 5 meters...
-
The D455 model has 2x the accuracy over distance of the D435 camera model. And the D415 model also has 2x accuracy of D435. So I use the green lower line on the diagram below as a rough visual gu...
-
The SDK has not officially supported Mac since 2018 and it has problems with modern MacOS versions such as Ventura and Sonoma. So Windows will be the preferable choice. Originally the RealSense ...
-
When processing is performed on the computer's CPU instead of the camera hardware, there is always a chance that performance may be negatively impacted. I cannot provide guidance on how much HDR m...
-
When HDR is enabled, it causes the infrared image to flicker rapidly (the depth image does not flicker). If you only need the depth image then enabling HDR should be the only step that you need to...
-
If your computer / computing device has a good enough hardware specification to not be noticeably slowed down by the processing burden of HDR then your save to files is not likely to be impacted.
-
The RealSense D455f camera model is equipped with a light-blocking filter on its lenses that is better able to deal with light reflections. https://www.intelrealsense.com/depth-camera-d455f/ If c...
-
If the camera returns to normal after covering the front of the camera then it can indicate that the left / right infrared sensors may have become saturated. This can occur in very dark or very br...
-
The V4 version of the D4 is used with a D401 depth module to form a D405 when joined together. V4 is not compatible with D450. If a D450 is used with the D4 V5 then a D457 is formed. The camer...