MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
RealSense 400 Series cameras are not interfered with by IR from non-RealSense IR devices but can interfere in return with those devices. For example, a nearby wireless mouse transmitter or an IR c...
-
Hi Arthur Levisalles10 The RealSense SR300 camera model was retired years ago but continued to be supported by the RealSense SDK alongside the newer generation 400 Series stereo depth camera range...
-
If you mean observing the chest rising and falling as the patient breathes then that should be fine, as the data will update in real-time.
-
You could certainly generate a pointcloud of the surface of the patient and read coordinates from those points. You can also measure distance between two or more points on the pointcloud. If you...
-
Hi Dnrdyd0379 This purple hue on the RGB image is a characteristic of the D455 model under certain outdoor lighting conditions. Intel provide advice about it on page 8 (the final page) of a PDF d...
-
Hi Scurry1624 I confirm that the D405 model does not have a set of hardware sync pins. If you have not already purchased the D405 cameras then the D435 model should be able to meet your sync and...
-
Hi Arthur Levisalles10 The D415 camera model would be an appropriate choice for this application. It has around 2x better image quality and 2x less depth error over distance than D435 and can be ...
-
I cannot provide a guarantee that changing the cable will solve the problem, but using a high quality cable can be helpful. RealSense cameras can use USB 2.1 or USB3 (USB 3.1 / 3.2). The interna...
-
Hi Sasabukreev808 As you are using a D410 depth module, you likely purchased your own USB cable for it. If it is your own choice of cable, it should be a high quality one that is designed for dat...
-
Aruco tags are black and white. https://docs.opencv.org/4.x/d5/dae/tutorial_aruco_detection.html