MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Thank you for the clarification. It sounds as though you are describing the Vision Processor D4 Board, which is one of two circuit boards inside the camera. The other board is the camera module t...
-
You are correct, if the JetPack is downgraded to 5.1 then installing the MIPI driver or using the libuvc backend installation method may not be necessary. However, in this situation using libuvc b...
-
I would recommend first trying the libuvc backend installation method It is possible that you can use your D455 on Jetson AGX Orin with JetPack 6 if you install the MIPI driver, but I cannot pro...
-
It is important to use an SDK version that is compatible with the firmware driver that is installed in the camera. The minimum recommended firmware version for D455 is 5.13.0.50. The SDK version ...
-
Hi Sasabukreev808 Could you provide more information about the microcircuit that you are describing, please? Thanks!
-
Hi Hassanshafi The IP65 casing that protects against entry from dust and water spray is the only difference between the D455 and D456 models.
-
There is not a definition available for what the malformed vid string error means. It seems to be an error that only occurs on Windows though, as it is part of the win-helpers.cpp file of the Real...
-
Hi G Krier Physical changes to RealSense products are published as notices months in advance of the change on Intel's Product Change Notification (PCN) website at the link below. There are curren...
-
1. Yes, if you have potential conflicts with your computer's kernel then I would always recommend building from source code with a method that enables librealsense to bypass the kernel. This woul...
-
1. The camera should not become inaccessible when the projector is shut off. VIDIOC_S_EXT_CTRLS errors indicate that there is likely a conflict between the program and the kernel version on your ...