D457 Infrared projector fails to restart after overheating shutdown
-
Hi Layth Mahdi What you describe is correct. The RealSense firmware driver contains a laser safety mechanism that shuts off the projector's laser if the internal Projector temperature of the camera exceeds 60 degrees C for several seconds.
The camera is able to continue operating when the projector is off, though there may be a decrease in detail on the depth image and the camera would be unable to see a real-world scene whose lighting is dim or dark.
The internal temperature of the camera is influenced by the temperature of the camera's casing. Intel lab tests found that the Projector temperature should not exceed 60 degrees C if the casing temperature does not exceed 44 degrees C. This test was on models preceding the D457 though that have a ventilation grille in their casing, whilst D457 has an environmentally sealed casing to defend against dust and water spray entry.
If the environment continues to severely heat the outer casing then it may be difficult for the internal temperature of the camera to fall.
You could write a program code routine to continually check if the IR emitter (i.e the projector) is disabled, and if it is AND the Projector temperature is < 60 then enable it. Both the emitter status and Projector temperature can be queried with code.
-
Hi Marty,
The issue is, when the IR projector goes off, we no longer see the camera through rs-enumerate-devices, so we cannot communicate with it. Although, we do receive point cloud information.
When we send rs-enumerate-devices, we get:
“ 22/07 15:59:27,950 ERROR [281473202063616] (librealsense-exception.h:52) xioctl(VIDIOC_S_EXT_CTRLS) failed Last Error: Invalid argument
22/07 15:59:27,950 ERROR [281473202063616] (rs.cpp:237) [rs2_create_device( info_list:0xaaab27f82190, index:1 ) Backend] xioctl(VIDIOC_S_EXT_CTRLS) failed Last Error: Invalid argument
22/07 15:59:27,950 ERROR [281473202063616] (rs.cpp:237) [rs2_delete_device( device:nullptr ) UNKNOWN] null pointer passed for argument "device"
Could not create device - xioctl(VIDIOC_S_EXT_CTRLS) failed Last Error: Invalid argument . Check SDK logs for details”The questions we have are:
1. Why we no longer see the camera if the projector is down?
2. Why can’t RealSense firmware automatically restart the projector if the right conditions were met. -
1. The camera should not become inaccessible when the projector is shut off. VIDIOC_S_EXT_CTRLS errors indicate that there is likely a conflict between the program and the kernel version on your computer. Building the librealsense SDK from source code with the libuvc backend method using a build script at the link below can enable it not to be dependent on specific Linux versions or kernel versions.
https://github.com/IntelRealSense/librealsense/blob/master/doc/libuvc_installation.md
2. I am not involved in RealSense firmware driver development and so cannot offer advice about this question, unfortunately.
-
1. We are using apt install librealsense2. Not sure what you mean by conflicting between the program and the kernel. Do you mean we should always compile from the source code rather than using the apt binary?
2. Who should we contact to potentially, include this in the next firmware? -
1. Yes, if you have potential conflicts with your computer's kernel then I would always recommend building from source code with a method that enables librealsense to bypass the kernel. This would be the libuvc method mentioned above, or the RSUSB backend method at the link below.
https://github.com/IntelRealSense/librealsense/issues/9931#issuecomment-964289692
2. I would strongly recommend addressing the issue by writing a checking routine in a program as suggested above, as a firmware feature request is not likely to be successful. It is significantly more complex to implement a change in the firmware driver than in the SDK's code, and new firmwares have to be tested very extensively before being cleared for release.
Please sign in to leave a comment.
Comments
5 comments