MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
There is not publicly available information available about the thermal resistance of heatsinks used with RealSense depth camera modules. I am not a member of the Intel RealSense Help Center foru...
-
Hello, I note that you are using version 2.39.0 of the RealSense Viewer tool, which is now very old. If your camera has a modern firmware driver installed in it then the camera is unlikely to work...
-
Hi Vroan The version is selectable from a 'Version' drop-down menu at the top of the page that you are taken to when clicking on the firmware link. Here is the link for the 5.15.1.0 download page...
-
Hi Steven Wilson The temperature information for the depth modules is at the bottom of page 50 of the current edition of the 400 Series data sheet document. I have quoted that section in the imag...
-
I suggested to attach a heatsink to the back of a D401 module. If your preference is to attach a heatsink to the back of the D401 module inside a D405 that you already have then the limited space ...
-
Hi, the Python script at the link below may be a helpful reference. https://github.com/IntelRealSense/librealsense/issues/6267
-
Hi Jooha Maeng If you are thinking of using a RealSense depth module board instead of a cased camera then the two circuit boards inside the D405 are available as the D401 depth module and the Visi...
-
When using RGB from the left infrared sensor it is not necessary to perform alignment. Because depth and the RGB from IR originate from the same sensor, the left IR image has the benefit of always...
-
Hi Alexchandriyaa If you are using the D457 in USB mode so that it is detected as a D455, the RealSense-compatible commercial skeleton tracking software Nuitrack SDK may be able to meet your needs...
-
Thanks very much for the update. As that particular camera works on Ubuntu computers and on a Windows laptop, and other cameras work on that computer, it could be an issue with the Windows operati...