RealSense Support

3D point cloud

Comments

6 comments

  • 19829127419

    What I mean is that the point cloud is determined the moment the infrared camera is turned on and will not change, but I need a dynamic point cloud generation effect when I am ready and then lock the generated point cloud.

    0
    Comment actions Permalink
  • MartyG

    Hello, I note that you are using version 2.39.0 of the RealSense Viewer tool, which is now very old.  If your camera has a modern firmware driver installed in it then the camera is unlikely to work well with an old Viewer version.

     

    You can check which firmware version is currently installed in your camera by clicking on the Info button at the top of the Viewer's options side-panel.  The recommended firmware for 2.39.0 is 5.12.8.200

     

    Depending on your camera model though, you might cause your camera to become non-functioning if you downgrade to such an old firmware version.

     

    I would recommend using the current latest 2.55.1 version of the Viewer if possible, and firmware 5.16.0.1.  If you are using Windows then you can use the 2.55.1 version of the Viewer by visiting the link below, going to the 'Assets' file list at the bottom of the page and downloading and running the file Intel.RealSense.Viewer.exe

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.55.1

     

     

     

    0
    Comment actions Permalink
  • 19829127419

    Thank you!MartyG. I have another question I'd like to ask you. For example, here is a depth image taken by a D435i camera. How can I convert it to 3D point cloud data using python code?Are there any python code examples for this?

    0
    Comment actions Permalink
  • MartyG

    There is an official Python pointcloud example called opencv_pointcloud_viewer.py at the link below.

    https://github.com/IntelRealSense/librealsense/blob/master/wrappers/python/examples/opencv_pointcloud_viewer.py

     

     

     

    0
    Comment actions Permalink
  • MartyG

    If your aim is to generate a point cloud from saved image files such as PNG then there are few references for doing so.  The RealSense article with Python scripting in the link below might be helpful though.  If you get a pop-up box suggesting that you register for the website then just click the 'X' in the corner of the box to remove the pop-up and view the article.

    https://medium.com/@mustafaboyuk24/obtaining-point-cloud-from-depth-images-with-intel-realsense-d-435-camera-144e8ef9260d

    0
    Comment actions Permalink
  • 19829127419

    MartyG, thank you so much! Your answer is very helpful to me.

    0
    Comment actions Permalink

Please sign in to leave a comment.