MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
By starting and stopping the unique pipeline of each individual camera, you are effectively toggling the cameras on and off in sequence instead of having all cameras capturing simultaneously. If ...
-
Hi Eli Dejou If you do not need to sync the cameras then you could not use hardware synchronization at all and instead use the D415 script at the link below that takes a single capture from all at...
-
No, do not uninstall the red one.
-
Sometimes an SR300 does not work if the Virtual Driver is missing and sometimes the Virtual Driver is missing but the camera still works. So I cannot say for certain that the absence of the Virtua...
-
Yes, the sticker shows the serial number. An SR300 camera can be used to access RGB with non-RealSense applications that use video even if the RealSense aspects of the camera such as depth sensin...
-
Hi Sxl1437280316 The SR300 camera model is a USB 3 device that requires a USB 3 port. Is your camera plugged into a USB 3 port on your computer if it has one, please? It will not be listed in th...
-
You can also define a threshold filter in the RealSense Viewer tool without requiring any programming. If you plan to use both RGB and depth and would like to exclude RGB detail by distance as we...
-
Hi Andrew John Madey If you do not require identification of specific objects, the most straightforward approach may be a C++, Python or C# language script in the RealSense SDK that applies a post...
-
Hi Matheus Soares Here is the information that you requested about the RealSense D457. 1. The Fakra cable in the D457 box has a length of 1000 mm +/- 10 2. According to RG174 coax cable spec...
-
Hi Steve Steve If your D455 can only attain 4 meters depth range in the RealSense Viewer then a post-processing filter called the Threshold Filter may be limiting it. This filter is used to set a...