D437 GMSL Cable
Hello,
How long is the coax cable that comes with the camera? How much is its bend radius?
-
Hi Matheus Soares Here is the information that you requested about the RealSense D457.
1. The Fakra cable in the D457 box has a length of 1000 mm +/- 10
2. According to RG174 coax cable spec, the minimum radius is 9.9 mm.

3. Users can obtain a longer cable from the market. It is recommended to use “LEONI Dacar 302” for a 10 ~15 m long cable. RG174 cable has been tried on D457. The maximum length is 11 m, but Dacar 302 can reach 15 m.
Please sign in to leave a comment.
Comments
2 comments