MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
It's great to hear that you were successful with the EtherSense tool! To customize resolution and framerate, you would likely have to edit the cfg stream configuration instruction on line 37 of t...
-
Hi Maren Pedroza The 0.25 health check score that you experienced applies to On-Chip calibration, whose purpose is to improve depth image quality. Tare calibration is focused on improving depth m...
-
2.53.1 should be fine. The EtherSense networking tool is supported in both latest and old SDK versions.
-
If you are using SDK 2.53.1 then the 2.53.1 version of pyrealsense2 is the appropriate one to use. I note that you installed with the pip install pyrealsense2 method. It looks as though it insta...
-
Yes, the above illustration shows the back of the module. You do not need to refer to the back of the depth module, or even the sensor lens. The vast majority of users simply use the unaltered d...
-
If you are using depth-to-color alignment then yes, the origin of depth changes from the center-line of the left IR sensor to the center-line of the RGB sensor and the RGB color intrinsics should b...
-
Hi St160743 The origin of RGB is the center-line of the RGB sensor. The RGB sensor does not measure distance, so the front glass measurement is only relevant to depth measurements. The origin of...
-
You are very welcome, Yasin! Please do reach out again if you have further questions. Good luck!
-
Hi Ykawate1 The water protection of the D456 and D457 models is rated as IP65, meaning that it protects against directional jets of water spray. https://www.intelrealsense.com/depth-camera-d456/ ...
-
Hi Noahmercier7 The model of visible pattern projector illustrated in the projector paper appears to be an AAXA M6 mini-projector. https://aaxatech.com/products/m6_pico_projector.html https://uk.pc...