MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
The easiest way to obtain an RGB sensor would be to use the D415 Depth Module Kit board. It is the only caseless board in the range that has the RGB sensor integrated onto its circuit board instea...
-
Dorodnic the RealSense SDK Manager said about T265 calibration: "The T265 comes precalibrated and does not require any user recalibration. If you want to integrate it with 3rd-party wheel-odometry...
-
Apologies for the delay in responding. I've been analyzing and considering the images very carefully to try to form an impression in my mind of what's happening. It looks as though you are pointi...
-
The Chief Technical Officer of the RealSense Group at Intel (agrunnet) mentioned it yesterday (5 Aug 2019) in the present tense, though it could have been a reference to a firmware that is in inter...
-
If the start-up problem is occurring when you restart the camera after having already started and stopped it before, it may be that the problem is occurring because the camera was not properly shut...
-
A quick way to apply settings in the 400 Series without hand coding them all is to set them in the RealSense Viewer and then export the settings in a 'custom preset' file that can then be loaded ba...
-
The speckles are likely generated by the IR Emitter component of the camera, which projects a semi-random pattern of dots onto a scene. Their visibility on the image can be reduced by reducing th...
-
The SR300 camera model used to work with OBS but also now has had problems reported with it. XSplit (the popular alternative to OBS) now has a program called XSplit VCam that does background remo...
-
You are totally welcome. That is awesome news - I'm really glad that your problems have been resolved. Thanks for letting us know! :)
-
Python 3.7 support was added in SDK version 2.23.0, the version before the one that you are using (2.24.0). https://github.com/IntelRealSense/librealsense/issues/4515 The official instructions for...