RealSense Support

Is it possible to use the PyRealSense2 wrapper using a USB2.0 port?

Comments

9 comments

  • MartyG

    If this error occurs, Dorodnic the RealSense SDK Manager has suggested trying another USB2 port or a different cable, or reducing the resolutions used in the sample code (due to the limited range of resolutions available on USB2).  The full discussion can be found at the link below:

    https://github.com/IntelRealSense/librealsense/issues/2818 

    0
    Comment actions Permalink
  • Rafael Calleja

    Unfortunately only one USB 2.0 port exists on the PYNQ board that I am working on and lowering the resolution in the sample code didn't fix the issue. Reading through the discussion, it doesn't seem like anyone confirmed that they could get the examples to work over a USB 2.0 connection. Does the RealSense team have any idea whether this configuration is supposed to work?

    Thanks for the quick replies!

    0
    Comment actions Permalink
  • MartyG

    My understanding is that you should be able to use USB2 so long as your code uses a resolution that is available to your board.  rs-enumerate-devices can provide a list of the resolution modes supported on your hardware.

    I would also recommend ensuring that the camera's firmware driver has an up to date version.

    0
    Comment actions Permalink
  • MartyG

    The comment that you posted here after this one seems to have disappeared, so I will paste it in below for the benefit of other readers.  Looking at the stream definition code you posted though, unless you have defined new values for the variables res_w and res_h, I would guess that they would still represent resolution values not compatible with USB2.   I would put the resolution values into the equation directly, like this:

    config.enable_stream(rs.stream.depth, 480, 270, rs.format.z16, 30)

    Also, I note that your camera identifies as a D400.   The color stream would not work in that case if it is a D400 caseless Depth Kit module board, as only the D415 (Module Kit or USB camera) or D435 / D435i (USB camera) have an RGB sensor.  The rest of the 400 Series range (400, 410, 420, 430) don't have an RGB sensor for color.  It is probably looking for a color mode that the camera doesn't support (note there are no color modes in the rs-enumerate-devices list) and may be erroring over that.

    ****************

    Your lost message:

    The rs-enumerate-devices command yields this output:

    Device info:
    Name : Intel RealSense USB2
    Serial Number : 828112070194
    Firmware Version : 05.09.02.00
    Recommended Firmware Version : 05.11.06.250
    Physical Port : /sys/devices/soc0/amba/e0002000.usb/ci_hdrc.0/usb1/1-1/1-1:1.0/video4linux/video0
    Debug Op Code : 15
    Advanced Mode : YES
    Product Id : 0AD6
    Product Line : D400
    Asic Serial Number : 829313021313

    Stream Profiles supported by Stereo Module
    Supported modes:
    stream resolution fps format
    Infrared 1 480x270 @ 30Hz Y8
    Infrared 2 480x270 @ 30Hz Y8
    Infrared 2 480x270 @ 15Hz Y8
    Infrared 1 480x270 @ 15Hz Y8
    Infrared 1 480x270 @ 6Hz Y8
    Infrared 2 480x270 @ 6Hz Y8
    Infrared 1 424x240 @ 30Hz Y8
    Infrared 2 424x240 @ 30Hz Y8
    Infrared 2 424x240 @ 15Hz Y8
    Infrared 1 424x240 @ 15Hz Y8
    Infrared 2 424x240 @ 6Hz Y8
    Infrared 1 424x240 @ 6Hz Y8
    Depth 480x270 @ 30Hz Z16
    Depth 480x270 @ 15Hz Z16
    Depth 480x270 @ 6Hz Z16
    Depth 424x240 @ 30Hz Z16
    Depth 424x240 @ 15Hz Z16
    Depth 424x240 @ 6Hz Z16


    When inputting these parameters into the pipeline config like so:

    config.enable_stream(rs.stream.depth, res_w, res_h, rs.format.z16, 30)
    config.enable_stream(rs.stream.color, res_w, res_h, rs.format.y8, 30)
    I still get the same error with no new information:

    RuntimeError Traceback (most recent call last)

    <ipython-input-8-b7ad4c41aed3> in <module>()

    1 # Start streaming

    ----> 2 pipeline.start(config)

     

    RuntimeError: Couldn't resolve requests

     

     

    0
    Comment actions Permalink
  • Rafael Calleja

    I guess when I edited the post to add the values for res_w and res_h it deleted it from the thread?

    I set correct values from the list given by rs-enumerate-devices. I got the depth camera to work, however the color stream still does not work. You said that the problem is that I have a D400 camera, and I understand that the device is registering as such as evidenced from the rs-enumerate-devices command, however I have the box right in front of me and the camera is indeed a D435.

    On another note, the depth camera seems to be working incorrectly as seen in the picture below. This is a depth colormap of me.

    0
    Comment actions Permalink
  • MartyG

    Ok, I think I mis-read the details.  The camera is identifying as USB2 (it would identify as 'D435' if it is a D435 model in a USB 3 port) and the D400 is referring to the '400 Series' RealSense product line, not the model number D400.

    I believe you should be able to access depth and color with USB2 on a D435.  The D435i model does not have color on USB2.  Can you confirm please that you have the D435 model, and not the D435i with an added IMU unit?

    The bad depth image on USB2 may be an indicator that the camera needs re-calibrating.   The Dynamic Calibrator tool can be downloaded from here:

    https://downloadcenter.intel.com/download/28517/Intel-RealSense-D400-Series-Calibration-Tools-and-API 

     

    0
    Comment actions Permalink
  • Rafael Calleja

    The camera is indeed a D435 and not a D435i. I will try the recalibration and attempt to access the color stream again. I'll post back whether or not the fixes work. Thanks for all the help!

    0
    Comment actions Permalink
  • Rafael Calleja

    @MartyG you are a life saver. The re-calibration fixed all my problems. I am now able to stream at a higher FPS with higher resolution and the recalibration also unlocked other color maps (i.e. RGB, YUYV). 

    I guess this confirms that it is indeed possible to develop using the Intel RealSense camera on a USB 2.0 port.

    Thank you so much!

    0
    Comment actions Permalink
  • MartyG

    You are totally welcome.   That is awesome news - I'm really glad that your problems have been resolved.  Thanks for letting us know!   :)

    0
    Comment actions Permalink

Please sign in to leave a comment.