MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
There has been a similar case this week where the user was connecting a T265 tracking camera to an Xavier and having detection problems after either hard or soft boot when connecting the camera dir...
-
You may achieve a darker image if you disable the IR Emitter component of the camera. This can be done in the RealSense Viewer or with scripting. If you plan to use the camera with Unity, below i...
-
I'm very pleased that the script met your needs. Thanks for the update!
-
It looks to me as though the work necessary for generating the frame for each stream may be occurring in the line preceding the app.show(render_frames) instruction: render_frames[frame.get_profile...
-
You could try some of the noise reduction suggestions for the D415 that I just posted on another case. https://github.com/IntelRealSense/librealsense/issues/4703#issuecomment-523823310 Point 2 is a...
-
I'm very glad to hear you got much improved performance by changing the USB cable. Thanks for updating us! Though your case of incomplete frames therefore seems related to the USB system, it is w...
-
I'm very glad that you were able to solve your problem, Gaurav. Have a great day!
-
Hello Gaurav, There are a number of different reasons why a recording may have missing frames. It could be related to a glitch on the USB port or USB cable, or something occurring on the particula...
-
There's no limit on the number of questions, so don't worry. :) The subject of custom firmware is answered in the link below by the Chief Technical Officer of the RealSense Group at Intel (agrunne...
-
If it were a Windows computer then access to the camera could be blocked by disabling it in the Privacy settings of Windows, and perhaps setting the control panel so that only a user with the right...