MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
You are very welcome. I look forward to your next update tomorrow!
-
Is he new camera the D415 board with the casing? If the D415 boards are both okay and the the D4 V1s are both okay, that could mean that one of the interposer cables that joins the D4 and D415...
-
Your English is very good, don't worry. The D4 board with the white sticker on is a V1. I confirmed this with the part code number on the sticker. The D4 board beside it without the sticker app...
-
Hello, are you using a Vision Processor D4 board and a D415 Depth Module board please? If you are using a Vision Processor D4 board with a D415 board, the D4 board needs to be the V1 version. Oth...
-
Then select the IMU topic in RViz2.
-
If the individual accel and gyro topics are published, can the messages be seen in RViz if you add unite_imu_method:=2 to your ROS launch command to combine the accel and gyro topics into a single ...
-
Does the IMU problem still occur if you reset the camera in the Viewer by going to the More option at the top of the options side-panel and selecting 'Reset Hardware' from its drop down menu? As ...
-
Please try inputting the command below into the Ubuntu terminal to delete the configuration file of RealSense Viewer, which will cause the Viewer to reset to its default settings next time it is la...
-
During our discussion we have not mentioned the USB cable. Are you using the official 1 meter cable supplied with the camera or another cable of your own choice, please? Could you try unplugging...
-
Do both Accel and Gyro display at the same time if you leave their speeds on their default frequencies - 100 for Accel and 200 for Gyro.