MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
If the D430 module was flexed during handling then it can negatively affect the calibration of the imager sensors. It is correctable though by re-calibrating the sensors. This can be done with th...
-
I am not on the developer team and so do not have the ability to debug this case, unfortunately. The best chance of giving the issue visibility is likely to be to post a new message there so that ...
-
Others have been experiencing the exact same problem with this program. There is currently an open case about it on the RealSense GitHub forum at the link below. Adding a comment to that discussi...
-
Intel are handling all T265 related questions on their RealSense GitHub forum. Please re-post your message there. I apologise for the inconvenience. You can post at the GitHub by visiting the lin...
-
I checked the most recent edition of the data sheet document for the RealSense 400 Series cameras (October 2019 at the time of writing this). At the end of the section on the flexible interposer c...
-
Though there are a lot of example programs in C++ language, I realised that you likely would prefer examples in Python. A selection of Python examples with source code are available in the link be...
-
The visibility of the projected dot pattern is tied to the value of the 'Laser Power' setting in the "Controls" section of the Viewer's options side-panel. The pattern becomes more visible when La...
-
If you are using the RealSense Viewer software that is installed on the computer when the RealSense SDK is installed, then you can set the streams that you want to be active by setting the box besi...
-
The best approach may be to set multiple filter types and configure the balance of their values so that it has the overall effect on your output image that you are seeking. The RealSense Viewer ta...
-
The Vision Processor D4 circuit board inside the camera performs adjustments such as "rectification" of the captured raw camera data and then sends the updated data through the USB cable to the com...