MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Could you check the connection between the D430 Depth Module board and the Vision Processor board to see if they are firmly attached? Are you using the rigid connector board or a flexible cable to...
-
One way to make a dark or reflective surface more readable by a depth camera is to use a fine spray-on powder on the surface, such as foot powder or baby powder. This is probably not a practical m...
-
RealSense cameras are sensitive to the state of the USB port due to the volume of data that they transmit through the USB cable. An individual RealSense camera can draw up to 2 watts of power, so ...
-
I see the quoted issue DSO-14558 is "Open" in the firmware release notes. The term 'open' means that it is being still assessed by the RealSense engineering team. As it is not labelled as 'Plan F...
-
Yes, it has been a Known Issue about the possibility of the camera not being detected after a "soft reboot" (restarting the computer instead of completely shutting it down and then restarting it wi...
-
For D415 and D435 cameras, a final stage that comes after scale calibration is RGB camera calibration. This may be what the application is crashing out at. The description in the guide sugges...
-
Awesome news - thanks for the update!
-
I hope that the colorizer code in the link below will solve your problem with these settings: https://github.com/IntelRealSense/librealsense/issues/5371
-
Other RealSense Android users have previously had problems with accessing the camera with Android 10. https://github.com/IntelRealSense/librealsense/issues/5388 A RealSense user in that discussion...
-
Ply files are a way of saving point cloud data into a permanent file. SLAM usually generates its point cloud data in real-time. So unless you are recording the data then it would be lost when the...