MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Information on bag files can be found here: https://github.com/IntelRealSense/librealsense/blob/master/doc/sample-data.md The RealSense Viewer program can record data from its "2D" mode into a bag...
-
If you are using image files (not live camera streams), the link below discusses aligning an rgb image file and a depth file and then calculating the measurements. https://forums.intel.com/s/questi...
-
If you are seeking to measure the complete dimensions of the object (its 3-dimensional volume), the RealSense SDK has an example program in the Python language called box_dimensioner_multicam. http...
-
Thanks for the question! I have posted a reply on the GitHub version of your question. https://github.com/IntelRealSense/librealsense/issues/5435#issuecomment-619154195 It would be difficult to o...
-
I re-read your case from the beginning and noted that the non-detection was not happening on every reboot, but on every second reboot. This is highly unusual. I have been handling another case on ...
-
Others have tried cutting lines in the cable to remove USB 2.0. It apparently worked for them too. https://electronics.stackexchange.com/questions/107669/usb3-with-fewer-wires I would personally...
-
I'm glad you found a solution, even if it required a change of server! The D435 is the best choice of the 400 Series for dark scenes, as it has a wider IR imager that can let in more light than the...
-
The next thing you could try is setting all of Windows' power-saving plans to "Never". You can find the power plan settings window by typing 'power plan' into the text box at the bottom of your Wi...
-
Okay, thank you very much. I believe that IC2 errors are an error with the camera hardware. If you can access the RealSense Viewer program, does the error get connected if you go to the 'More' ic...
-
The D430 is a camera circuit board module without a casing. Did you mean that you have a D435 camera, please?